Reply
Posts: 4
Registered: ‎03-09-2017

Si8902 SDO pin HIGH when EN# line is high

From the datasheet the SDO output pin should enter high-Z when EN is high.  I have tried 3 different chips, and all of them have high SDO pin.  Exept of this, the SPI communication is ok.  VDDA and VDDB is +3V3.  Any suggestions? 

Posts: 3,097
Registered: ‎02-07-2002

Re: Si8902 SDO pin HIGH when EN# line is high

How did you measure this pin is high? Have you tried adding a 10k pulldown? Is it still high then?

Posts: 4
Registered: ‎03-09-2017

Re: Si8902 SDO pin HIGH when EN# line is high

I have tried connecting a 10k pulldown and it's still high. 

Posts: 3,097
Registered: ‎02-07-2002

Re: Si8902 SDO pin HIGH when EN# line is high

Ok. I just wanted to check your conclusion.

 

I guess a SiLabs employee needs to answer this now. If you don't get an answer here, try opening a support ticket. And if you get any answers, please report back here for others to find.

Posts: 4
Registered: ‎03-09-2017

Re: Si8902 SDO pin HIGH when EN# line is high

Answer from SiLabs:

The Si89xx has no enable pin, so the SDO output is a push-pull output with no pull-up. If you need tristate or OD output, you will need a tristate buffer or OD buffer.

Datasheet:

EN Rising to SDO High-Z tSDZ — — 160 ns.

Posts: 4
Registered: ‎03-09-2017

Re: Si8902 SDO pin HIGH when EN# line is high

Updated SiLabs answer:

I have learned that the SPI bus on this part is not compliant, and will not release SDO. The data sheet will be revised. You will need a tristate or OD buffer in order to share the line.