Reply
Posts: 10
Registered: ‎05-08-2017
Accepted Solution

SI4713 + I2S

[ Edited ]

I currently have the SI4713 working using analog audio but I would like to use I2S which I have been unable to get working.

 

I use the following commands to configure the device uniquely for I2S.

 

POWER_UP  -- arguments 2, 0x0f -- for Xmit and Digital Audio

 

DIGITAL_INPUT_FORMAT - argument 8 -  for DCLK Raising edge, I2S mode, Stereo, and 16 bit audio

 

DIGITAL_INPUT_SAMPLE_RATE - argument - 44100

 

Can someone enlighten me as to what I'm missing?

 

Is there a requirement for a specific sequence of commands that must be met?

 

Thanks in advance for any comments.
 

Posts: 10
Registered: ‎05-08-2017

Re: SI4713 + I2S

Is this forum strictly for fellow users to help each other or do experts from SI also comment to answer questions?

Posts: 10
Registered: ‎05-08-2017

Re: SI4713 + I2S

Update:

 

I received an email from Andreq Zeng (SI) today stating the following:

 

"you need to establish DCLK and DFS prior to enabling the digital audio output by setting DIGITAL_OUTPUT_SAMPLE_RATE." ... I think he meant DIGITAL_INPUT_SAMPLE_RATE

 

That was the issue as I was setting up the SI4713 before starting I2S.

 

I start I2S - then initialize the SI4713 and it works as expected.

 

AN332 speaks to setting DIGITAL_INPUT_SAMPLE_RATE to zero prior to removing DCLK but no statement that DCLK needs to be present before setting it.  ---- Should be added to AN332.

 

Thanks Andrew.

 

Joe