Reply
Posts: 4
Registered: ‎03-06-2016

SI4688 EPAD conection.

[ Edited ]

Hi. What is a purpose of EPAD in SI4688 radio receiver? If I don't connect it to GND will the device work?
I have a problem in my device with loading image from host and i realized that i do not put pasta on EPAD. Could it be reason of malfunction?

Thanking you in advance,

Marcin.

Posts: 77
Registered: ‎02-15-2015

Re: SI4688 EPAD conection.


Marcin_Postek wrote:

Hi. What is a purpose of EPAD in SI4688 radio receiver? If I don't connect it to GND will the device work?


This central pad definitely needs to be connected to GND in order for the chip to work properly.

 

Best regards,

Andi

Highlighted
Posts: 4
Registered: ‎03-06-2016

Re: SI4688 EPAD conection.

My problem was on software side. I had automatic "chip select" "on" on my raspberry. So, I think device will work without this pad connected, but of coure not too well.