Reply
Highlighted
Posts: 4
Registered: ‎03-06-2016

SI4688 EPAD conection.

[ Edited ]

Hi. What is a purpose of EPAD in SI4688 radio receiver? If I don't connect it to GND will the device work?
I have a problem in my device with loading image from host and i realized that i do not put pasta on EPAD. Could it be reason of malfunction?

Thanking you in advance,

Marcin.

Posts: 65
Registered: ‎02-15-2015

Re: SI4688 EPAD conection.


Marcin_Postek wrote:

Hi. What is a purpose of EPAD in SI4688 radio receiver? If I don't connect it to GND will the device work?


This central pad definitely needs to be connected to GND in order for the chip to work properly.

 

Best regards,

Andi

Posts: 4
Registered: ‎03-06-2016

Re: SI4688 EPAD conection.

My problem was on software side. I had automatic "chip select" "on" on my raspberry. So, I think device will work without this pad connected, but of coure not too well.