Reply
Posts: 1
Registered: ‎03-07-2017

Multiple Output Voltages with SI882XX DC-DC Converter

I am looking for a simple solution to get an additional isolated auxiliary output voltage (>=11V, >=25mA) for powering a signal conditioning circuit on the isolated side.

Is there a suitable "off the shelf" transformer for this problem? I don't think that i'm the only one who needs another voltage than 5V on the secondary side, but I haven't yet found something suitable.... 

Highlighted
Posts: 13
Registered: ‎02-25-2014

Re: Multiple Output Voltages with SI882XX DC-DC Converter

There is no off-the-shelf solution for your requirement. We only support what we have in the data sheet.