Reply
Posts: 4
Registered: ‎10-25-2015

Is there method of restoring the original firmware in si4705-d60​-evb?

[ Edited ]

After I change the firmware of mcu(C8051F342)  in evb, is there method of restoring the original firmware?

 

Posts: 204
Registered: ‎09-16-2015

Re: Is the method of restoring the original firmware in si4705-d60​-evb?

I did not understand your question here.
are you asking the method to Flash the STK?
you could flash the MCU on the DK board any firmware you want.
if you have the original firmware, you could flash it into the MCU any time.

Highlighted
Posts: 4
Registered: ‎10-25-2015

How to restore the original firmware to mcu in si4705-d60​-evb?

[ Edited ]

I hope I could get the original firmware source.of si4705-d60​-evb.

I want to restore the original firmware by using its source.

I would also like to take advantage of the source code on the product being developed.

Thank you.