Reply
Highlighted
Posts: 2
Registered: ‎02-06-2016

Is the CP2112 Windows DLL source code available if I need to port to a different OS ?

Is the CP2112 Windows DLL source code available if I needed to port to a different OS

(ie. real-time OS) ?

 

How many copies of the CP2112 have you tested on a single PC at the same time ? Are

they all accessible ?

 

Randy

Posts: 2,198
Registered: ‎10-14-2014

Re: Is the CP2112 Windows DLL source code available if I need to port to a different OS ?

I suggest you create a ticket in our salesforce system

http://www.silabs.com/support/Pages/default.aspx

.

As far as I know to get some source code like this you need sign NDA.

It is more convenient  to discuss more in detail on this topic if you could create a ticket in salesforce.

My views are my own and do not necessarily represent the views of Silicon Labs

 

WeiguoLu