Reply
Posts: 1
Registered: ‎07-13-2016

FrameGrabber control problem

Hello,

 

I'm trying to write a c++ program in Visual Studio to control the FrameGrabber. So far the only thing I do is 

 

Fg_struct* fg = Fg_init("Acq_SingleCXP6x4AreaGray.dll",0);

 

And I get an application cannot start error.

I can compile and build the program but I cannot run it. I have already link the fglib5.lib library and included the .h files. But what I don't know is where should I put the .dll file. Now I have my dll file in the same folder as my project. I really don't understand why it is not working.

 

This is what I have in Additional Include Directories: $(SISODIR5)\include;$(SISODIR5)\include\msinttypes;..\..\include;..\..\CXP\CXPCommon;%(AdditionalIncludeDirectories)

 

I also copied the include and lib folder into my project.

 

Thanks.

 

 

Highlighted
Posts: 2,384
Registered: ‎10-14-2014

Re: FrameGrabber control problem

@sandraD
what device are you using that from Silabs?
WeiguoLu