Reply
Highlighted
Posts: 2
Registered: ‎07-21-2016

About using Si8244 in full bridge mode

Hello,

 

I am currently in the prototype phase of design of a Class-D amplifier using the Si8244. The design is based on the the reference design Si824xClassD-KIT​.

 

As the next phase of my design, I would like to design a dual supply, full bridge amplifier using 2 x Si8244.

Is there a reference/concept/ block-diagram design of the same that I can refer to?

 

Is SL planning to release a full bridge version of Si8244?

 

Thanking you in anticipation and awaiting your early reply.

 

Regards,

 

Ravindra Desai.