Reply
Posts: 1
Registered: ‎03-14-2017

Si7055 measured Temperature to high

[ Edited ]

I use the SI7055. When I read the temperature, this is 3 ~ 4 ° C higher than the ambient temperature directly next to the sensor. I measure with 11bit.

What is the cause of this?

 

kind regards

Dieter

 

Posts: 67
Registered: ‎04-09-2015

Re: Si7055 measured Temperature to high

The most common reason for readings higher than expected is heating from other components on the PCB. Please check if this could be the reason.