Reply
Posts: 1
Registered: ‎12-10-2015
Accepted Solution

Is the electronic serial number functional in devise Si7053 ?

I read correctly (CRC correct) the digits SNA_3 to SNA_0 and SNB3, but  SNB_2 to SNB_0 return to 0xFF with CRC faulty.

I have the same problem with Si7021 on Happy Gecko board.

Is there any hiden trick ? 

Highlighted
Posts: 59
Registered: ‎04-09-2015

Re: Is the electronic serial number functional in devise Si7053 ?

0xFF is normal for the other bytes. the CRC should be correct, but you do not need to worry about that.