Reply
Posts: 16
Registered: ‎01-20-2015

Incandescent lamp make PS reading unstable on Si1143?

I am using 1143 to make gesture detection and met a problem with Incandescent on.When I put the Incandescent lamp on, the variance of PS reading increase to 260. With Incandescent off, the variance is less than 50. Distance between Incandescent and Si1143 is around 30cm. Setting of Si1143 is as below:small IR photodiode, PS RANGE=0, default gain. Lux value of Incandescent lamp is ~1000(measured with an Lux Meter). I add the IRCompensation in my program(reference from slider demo code) and use below setting for IRcorrectionfactor. // Lg PD, PSRANGE = 0 // use { 17, 35, 29 } But after compensation, PS reading still changes a lot. Anyone have experience on this, Please advise. Thanks.
Posts: 8,068
Registered: ‎08-13-2003

Re: Incandescent lamp make PS reading unstable on Si1143?

you need a DC powered lamp, AC powered will make the intensity vary at 50/60 Hz

erik
Posts: 16
Registered: ‎01-20-2015

Re: Incandescent lamp make PS reading unstable on Si1143?

Thanks,erikm. Is there any reference that works on AC powered Incandescent? Filtering works?
Highlighted
Posts: 8,068
Registered: ‎08-13-2003

Re: Incandescent lamp make PS reading unstable on Si1143?

sample the AC, detect a precise place on the curve, synchronize your readings with that

erik