Reply
Highlighted
Posts: 2
Registered: ‎08-12-2015

I want to read "IR" values using SLSTK3201A kit (Will buy) or Sensor Puck (I have it).

I want to read "IR"/UV/Ambient/Hum/Temp using SLSTK3201A kit (Will buy) or Sensor Puck (I have it). I have read docs/literature but apparently the kit or puck apps has no mention of IR reading while sensor is capable of it. Dear Community, please guide how to start with and get the readings?

Posts: 327
Registered: ‎09-22-2009

Re: I want to read "IR" values using SLSTK3201A kit (Will buy) or Sensor Puck (I have it).

The sensor puck app does not have the ALS IR reading displayed, but the code running on the sensor puck MCU has access to the Si114x ALS IR data through i2c. If you got the SLSTK3201A, you would also do a similar process and have to go into the host MCU code (Zero Gecko) and access the data registers over i2c. The Si114x datasheet describes how to configure the device to take ALS IR measurements as well.