Reply
Highlighted
Posts: 10
Registered: ‎07-08-2016

Can I connect the Si1144 Heart Rate Sensor with the arduino hardware?

I have the Si1144-AAGX HRM sensor and I need it to connect to the "arduino uno-nano" development kit, its for my school project.

so is it possible? or i need the HRM-WG-BIO-44 development kit?

Posts: 10
Registered: ‎07-08-2016

Re: Can I connect the Si1144 Heart Rate Sensor with the arduino hardware?

upp

Posts: 18
Registered: ‎03-21-2014

Re: Can I connect the Si1144 Heart Rate Sensor with the arduino hardware?

Hi,

The SI1144 is intended for commercial use only.  If you're a student doing a project, we recommend using the Biometric Sensor Expansion Card: http://www.silabs.com/products/sensors/Pages/biometric-exp-evb.aspx.

 

This can be purchased from our website or from some catalog ditributors.