Reply
Posts: 9
Registered: ‎07-31-2015

relocation failed: value out of range or illegal

I have encountered an error while building my application for EM3588 on IAR. Does anyone know how to solve the linker issue?

 

Error[Lp002]: relocation failed: value out of range or illegal: 0x217f8
Kind : R_ARM_THM_JUMP11[0x66]
Location: 0x080056c4
Module: C:\Users\Antonio\Ember\EmberZNet5.6.0-GA\app\builder\meshsmart_node_firmware\build\obj\faults.o
Section: 8 (.text)
Offset: 0x0
Target : 0x08026ec1
"fault"
Module: C:\Users\Antonio\Ember\EmberZNet5.6.0-GA\app\builder\meshsmart_node_firmware\build\obj\faults.o
Section: 15 (.text)
Offset: 0x1

151 758 bytes of readonly code memory
23 446 bytes of readonly data memory
22 723 bytes of readwrite data memory

Errors: 1
Warnings: none

Link time: 0.76 (CPU) 0.76 (elapsed)
Error while running Linker

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 225
Registered: ‎02-13-2017

Re: relocation failed: value out of range or illegal

Which IAR version do you use?

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen