Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> ant
Posts: 11
Registered: ‎04-01-2016
Accepted Solution

how to get router table in border router?

dear sirs:

    we want to get the Whole Network Connectivity Diagram and debug the lost node which also rejion network.and I call emberGetRipEntry api with index is 0xFF,but the border router is crash:

 

Reset info: 0x0A (FAULT)
node type: 0x02
extended pan id: >4F8EC75FB4E1EFC6

 

please tell us how to get the Whole Network Connectivity Diagram to check thread network connecting info in border router?

 

tks

Posts: 188
Registered: ‎02-05-2014

Re: how to get router table in border router?

Which Silicon Labs Thread stack version are you using? Does this happen with the latest release (2.2.0) as well?

--------
The views represented in this post are the independent views of the author and don't necessarily represent the official views of Silicon Labs.
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> ant
Posts: 11
Registered: ‎04-01-2016

Re: how to get router table in border router?

dear sir:

   I used thread 2.1.1.0,and border router is v0.6.0!

 

tks