Reply
Posts: 2
Registered: ‎08-17-2016

how to change tx power dynamically especially for zigbee end device

I think a low RF tx power should be enough in the case that the zigbee end device is close to the gateway (coord) device, hence  it would be better for power saving if the TX power can be dynamically programmed. The adjustment can based on the LQI or RSSI. I've found this post about this issue:

 http://community.silabs.com/t5/Mesh-Knowledge-Base/Setting-ZNET-Channel-Tx-Power/ta-p/184398

 

it mentioned the emberAfPluginNetworkFindGetRadioPowerForChannelCallback defined by the network-find plugin, but I found it can only be used at the point device joining the PAN, after that this callback will not be called again, which doesn't satisfy my 'dynamically' requirement.

 

another API: emberSetTxPowerMode(uint16_t txPowerMode),  I'm not sure whether it can be called anytime when stack is up.

 

 

 

 

 

Posts: 85
Registered: ‎11-16-2015

Re: how to change tx power dynamically especially for zigbee end device

Hi Richard,

Silicon Labs ZigBee radios do not allow for dynamic changing of the radio transmiter settings dynamically.  While you can change the settings on the radio (Channel and power) at run time, the radio must be turned off and then back on for the settings to be changed.  For near dynamic changing you could cycle the radio power quickly to allow the Tx changes to be set.