Reply
Highlighted
Posts: 72
Registered: ‎06-02-2016

Zigbee callback on target device after binding?

[ Edited ]

 Hello,

 

I am using Ember Stack 5.7.2 and I need to notify the binding success or failed on the target device. I am not getting any callback on the target device side for binding success/fail/timeout.

 

Can anyone tell me, is there any way or callback to handle binding success on target devices?

 

Regards,

Sowmya

Posts: 11
Registered: ‎05-24-2016

Re: Zigbee callback on target device after binding?

Hi,

 

Depends on which type of binding you are using the response maybe different.

 

If you are using ZDO Binding process, the callback is a ZDO binding success callback.

 

Thanks.

Posts: 72
Registered: ‎06-02-2016

Re: Zigbee callback on target device after binding?

Hi,

I am using "Find and bind target" plugin. But I am not able to get which callback to use ? Can you please guide me.

Regards,
Sowmya
Posts: 120
Registered: ‎11-06-2014

Re: Zigbee callback on target device after binding?

Hi Sowmya,

 

The "Find and bind target" plugin provides the functionality for a target device to start identifying on user defined endpoints. The target device can then act as a target for a finding and binding initiator. The binding is then created on the initiator, not the target.

 

Best regards,

Yuping

Posts: 72
Registered: ‎06-02-2016

Re: Zigbee callback on target device after binding?

Hello Yuping,

 

Thank you for the information.

Yes initiaotor is holding the binding table to control the target. But if I need to display the target device binding success, which method do I have to use?

 

Regards,

Sowmya