Reply
Posts: 27
Registered: ‎04-06-2017

Which attribute can be reported in Zigbee?

For example, I found in ZCL spec, the cluster id :0x0001 (power configuration), the attr id 0x0021 (BatteryPercentageRemaining) could be reported. But for attr id 0x0020 (BatteryVoltage), the spec does not say whether it can be reported or not. And I also tried to configure reporting, it succeed. So my question is which attribute can be reported?
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 181
Registered: ‎02-13-2017

Re: Which attribute can be reported in Zigbee?

As I know, all of attributes can be reported. In ZCL specification, it only specifies if the attribute is for read only or for both read and write.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen