Reply
Posts: 26
Registered: ‎04-06-2017

Which attribute can be reported in Zigbee?

For example, I found in ZCL spec, the cluster id :0x0001 (power configuration), the attr id 0x0021 (BatteryPercentageRemaining) could be reported. But for attr id 0x0020 (BatteryVoltage), the spec does not say whether it can be reported or not. And I also tried to configure reporting, it succeed. So my question is which attribute can be reported?
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 120
Registered: ‎02-13-2017

Re: Which attribute can be reported in Zigbee?

As I know, all of attributes can be reported. In ZCL specification, it only specifies if the attribute is for read only or for both read and write.