Reply
Posts: 76
Registered: ‎05-19-2016
Accepted Solution

Unable to pair SLWSTK6000B with RD0051

Hi. Have the SLWSTK6000B kit -> able to run the Z3Light & Z3Switch together fine.

 

Should the Z3Switch be able to pair with the ref design RD0051 which is also Zigbee? The green light on the RD0051 continues to slowly blink and fails to pair up with the Z3Switch. Likewise, the console output on the Z3Switch is unable to locate a partner.

 

What are we doing wrong?

 

RD0051 was sourced in the last 48 hours from Digikey. This power plug is able to manually toggle the internal relay via the pushbutton.

Posts: 76
Registered: ‎05-19-2016

Re: Unable to pair SLWSTK6000B with RD0051

Perhaps answering my own question...in building the Z3Switch code, selected the SOC library and believe it should be the HOST library.

 

Will try again upon reaching the office.

Highlighted
Posts: 76
Registered: ‎05-19-2016

Re: Unable to pair SLWSTK6000B with RD0051

Update - RD0051 is for HA 1.2 compliant tools. Respectively have incoming the Wifi / Zigbee gateway reference design to allow for device binding of the switch IP and smart plug. This new tool should permit the proper operation of these components.