Reply
Posts: 5
Registered: ‎10-06-2016

Thunderboard Sense Thread and/or Zigbee examples

Are there any example code for the Thunderboard sense using Thread or Zigbee. If not can someone point me to instructions on how to set up Simplicity Studio to use the Zigbee/Thread SDK. I can not seem to get that working.

 

Thanks

Posts: 73
Registered: ‎06-17-2014

Re: Thunderboard Sense Thread and/or Zigbee examples

As far as I know, you need the IAR Embedded Workbench to use Thread and ZigBee stacks.

 

Michael

Highlighted
Posts: 5
Registered: ‎10-06-2016

Re: Thunderboard Sense Thread and/or Zigbee examples

So to use Thread on a 30$ dev board I have to shell out for a licence to IAR? 

Posts: 7
Registered: ‎10-20-2016

Re: Thunderboard Sense Thread and/or Zigbee examples

It seems like developing for Bluetooth also requires an IAR toolchain. Is that true?

Posts: 48
Registered: ‎11-07-2015

Re: Thunderboard Sense Thread and/or Zigbee examples

Sad but true.

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru
Posts: 48
Registered: ‎11-07-2015

Re: Thunderboard Sense Thread and/or Zigbee examples

Yes, IAR also requied for Bluetooth stack

 

From this link:

 

Note: IAR Embedded Workbench is required for ZigBee, Thread and Bluetooth Low Energy Development. A 30-day trial license for IAR Embedded Workbench for ARM is available with the EFR32 Mighty Gecko Wireless Starter Kit.

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru