Reply
Posts: 6
Registered: ‎02-17-2016

Thread: getting Routing table info

Hi,

 

Can you please share info on how to get routing table entries of a router node in thread?

 

we tried with EmberGetRipEntry(),  but not successful. please share sample code snippet.

 

Thank You,

Satish

Posts: 154
Registered: ‎03-31-2014

Re: Thread: getting Routing table info

Hello Satish,

emberGetRipEntry is described in ./stack/include/network-management.h. This can be used in combination with emberGetRipEntryReturn. Please note that this table does change without notice, sometimes frequently, and it gives only a partial view of the network. We do not recommend using it.

What is your use case?

 

Cheers,

Konrad

Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> ant
Posts: 11
Registered: ‎04-01-2016

Re: Thread: getting Routing table info

dear kpszupin:

    I got the same issue,we want to get the Whole Network Connectivity Diagram and debug the lost node which also rejion network.

   and I call emberGetRipEntry api with index is 0xFF,but the border router is crash:

 

Reset info: 0x0A (FAULT)
node type: 0x02
extended pan id: >4F8EC75FB4E1EFC6

 

please tell us how to get the Whole Network Connectivity Diagram to check thread network connecting info?

 

tks