Reply
Posts: 9
Registered: ‎06-27-2016

Simplicity Studio Thread GUI

Hello,

using the latest Gecko SDK Suite (v1.1.1) i cannot find anymore the hardware configurator in the Silicon Labs Thread GUI (Simplicity Studio .isc editor, HAL Tab). I have a custom EFR32 board an i'd like to write the firmware of a Thread end device, but how can i define the pinout and EFR32 interfaces (I2C, Timers, and so on)?

Posts: 181
Registered: ‎03-31-2014

Re: Simplicity Studio Thread GUI

Hello Leonardo,

 

The Hardware Configurator was deprecated in the Gecko SDK Suite (1.1.x). We have a guide for the new HAL config file format here: Migrating to the new HAL Config file format for EFR32