Reply
Posts: 1
Registered: ‎08-04-2015
Accepted Solution

Orphan Notification and Coordinator Realignment messages

I am using EmberZNet5.7.2-GA on EM357s.  

 

How can I...

1. In the ZED (or SED, sleepy end device) ensure that the Intra Pan is set to true in the Orphan Notification message? Currently it is set to false.

IntraPan=True.PNG

2. In the Coordinator Realignment response, ensure the Ack Required is set to true? Currently it is false.

 AckReq=True.PNG

 

Thanks,

Gary.

Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 181
Registered: ‎02-13-2017

Re: Orphan Notification and Coordinator Realignment messages

They are handled by EmberZnet and I don't think you can control this from application.
If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen