Reply
Posts: 2
Registered: ‎08-15-2017

Network Simulation

[ Edited ]

Hallo,

I'm currently evaluating different mesh technologies like ZigBee, Thread and BLE mesh.
I wonder if there are possibilities to simulate wireless networks given one of these protocols running on a particular board using some kind of hardware emulation.
I've already read about Cooja, Opnet and Omnet but I haven't discovered any solution yet.

Thank you in advance.

Cheers, Arne

Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 225
Registered: ‎02-13-2017

Re: Network Simulation

As I know, there is no such simulation tool.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen