Reply
Posts: 1
Registered: ‎10-05-2017
Accepted Solution

Network Analyzer with USB virt GW?

Hello,

 

Sorry if this is a duplicate post but I can't find any specific answer to the following question.

 

Can the Zigbee USB Virtual Gateway stick (RD-0002-0201) be used with Simplicity Studio (v4) as a network capture device?

 

I only have a RD-0002-0201 today with the default NCP software. I do not currently have an ISA3 JTAG programmer.

 

If anyone could confirm this is or is not possible (or if possible, what additional equipment I would need), that would be great.

 

Thank you,

-Brenton

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 225
Registered: ‎02-13-2017

Re: Network Analyzer with USB virt GW?

As I know, RD-0002-0201 cannot be used with Simplicity Studio (v4) as a network capture device.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen