Reply
Posts: 3
Registered: ‎07-07-2015

NCP giving back bad eui64?

It appears that when I have several nodes attached 10-12 or more I get back a bad eui64 when doing an "zcl global read 8 0"  which executes emberLookupEui64byNodeID().  Its approximately 10% of the time.  If I have fewer nodes all come back OK.

Highlighted
Posts: 147
Registered: ‎11-06-2014

Re: NCP giving back bad eui64?

Hi mars_wright,

 

Could you share a packet trace to demonstrate the problem? I'd like to see the packet details and investigate more. If you don't want to share the trace in public, please feel free to provide it via the support portal.

 

Thanks,

Yuping