Reply
Highlighted
Posts: 4
Registered: ‎03-30-2017

Mighty Gecko starter kits - what is the difference

Hello,

I was wondering what the difference is between the Mighty Gecko starter kits SLWSTK6000A and SLWSTK6000B?

I want to buy one of these so that I can develop a Zigbee lighting control device but I'm unsure which starter kit is best.

Thanks,

Neil
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 159
Registered: ‎02-13-2017

Re: Mighty Gecko starter kits - what is the difference

You can refer to http://www.mouser.tw/new/Silicon-Laboratories/silabs-mighty-gecko-mesh-devkit/ for the difference between SLWSTK6000A and SLWSTK6000B.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen
Posts: 133
Registered: ‎09-25-2015

Re: Mighty Gecko starter kits - what is the difference

I answered this in the portal case, but should have put it here, too, sorry about that.

 

The SLWSTK6000B is our updated kit, although the A may still be available depending on your distribution channel. The difference is that B uses radio boards with our newer EFR32MG12 parts (also featuring some cool capacitive sensors on the radio boards), and A uses EFR32MG12 parts, which only have 256 K of memory. If you are planning to do Thread or multiprotocol projects, then you should definitely get the B kit, but in most cases, you can make do with the A kit if it is more available.

Best,
-Alex