Reply
Posts: 2
Registered: ‎03-01-2017
Accepted Solution

Local storage application bootloader on EM3587

I'd like to implement application bootloading using local storage on an EM3587, as described in AN772 and UG103-6. I'm having trouble figuring out how to implement the local storage side - specifically how to write the new image into the top half of local flash. I believe that it's a matter of setting up a halBootloaderAddressTable, then calling the appropriate hal API's in bootloader-interface-app, but the specifics are escaping me...

 

Any hints, documentation, or example code would be greatly appreciated!

 

Highlighted
Posts: 144
Registered: ‎11-06-2014

Re: Local storage application bootloader on EM3587

Hi mkblackwell,

 

By "top half of local flash" you mean the higher-addressed half, right? With the local storage bootloader, the application is already configured to use the upper half as download space, and you don't need to do anything additional. Just make sure you select the local storage bootloader as the bootloader type when you build the application at the OTA client side, and have these plugins enabled:

OTA Bootloader Cluster Client

OTA Bootloader Cluster Client Policy

OTA Bootloader Cluster Common Code

OTA Bootloader Cluster Storage Common 

OTA Cluster Platform Bootloader 

OTA Simple Storage EEPROM Driver

     - Check SOC Bootloading Support. You can leave other configurations as defaults.

OTA Simple Storage Module

 

Best regards,

Yuping Xiao

Posts: 2
Registered: ‎03-01-2017

Re: Local storage application bootloader on EM3587

Thanks Yuping! The concept I was missing is that the application (via bootloader-interface) uses the halBootloaderAddressTable (and thus all the storage access functions) directly out of the bootloader, and you don't need to provide it separately. I have it working now with no problems - simple once I understood how it all fits together!

 

Posts: 144
Registered: ‎11-06-2014

Re: Local storage application bootloader on EM3587

Hi mkblackwell,

 

Glad to hear you got it working!

 

Cheers,

Yuping