Reply
Posts: 26
Registered: ‎04-06-2017

How to use motion sensor(IAS zone)

I'm using a motion sensor (IAS zone), but I can not understand the step how it works. I only know some steps should be done. (1) client send enroll response to server (2) server send enroll request (3) cleint write the IEEE address to server then server will report the open/close status to server. What is the correct sequence of (1)(2)(3)? Or there are some steps I have lost. Thank you!
Posts: 26
Registered: ‎04-06-2017

Re: How to use motion sensor(IAS zone)

Sorry my mistake, I'm using a door sensor not a motion sensor.
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 120
Registered: ‎02-13-2017

Re: How to use motion sensor(IAS zone)