Reply
Posts: 1
Registered: ‎12-05-2016
Accepted Solution

FreeRTOS port for EM3588

 

Hello.

Are there any known FreeRTOS ports for EM3588?

Thanks

Alex.

Highlighted
Posts: 179
Registered: ‎02-05-2014

Re: FreeRTOS port for EM3588

This can't really be done (at least in a way that integrates with the EmberZNet or Silicon Labs Thread stack) without access to underlying HAL library source code maintained by Silicon Labs because the stack relies on things like NVIC control and some system level ISRs for stuff like the radio, the flash controller, and the system tick that are managed in the HAL library.

 

It's certainly possible for Silicon Labs to do this in a way that integrates the stacks into FreeRTOS, but I don't think that's on the roadmap right now.  Any RTOS development is most likely going to be around the Micrium µCOS-II or µCOS-III RTOS kernel now that Silicon Labs has acquired Micrium.

--------
The views represented in this post are the independent views of the author and don't necessarily represent the official views of Silicon Labs.