Reply
Posts: 5
Registered: ‎04-19-2016

Force remove power off zigbee node?!

I have two question about this problem:

- Are this node will force remove automatic by Ember ZNet stack or must use some mechanism in Application (ie, store its network address, then send Leave command if received any message from this node,...)

- And, if the node I want to remove from network powered after timeout off Leave(s) command, is this still transmission messages with Coordinator (or other nodes)?

Many thank,

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 120
Registered: ‎02-13-2017

Re: Force remove power off zigbee node?!

If you enable Zigbee 3.0 child aging in your coordinator and routers, it would age out the device that doesn't do polling or send message for a period.

Posts: 5
Registered: ‎04-19-2016

Re: Force remove power off zigbee node?!

Hi YK,

No, The node (I want to force remove) can still send messages to the coordinator. The problem is I want to force remove power off node.

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 120
Registered: ‎02-13-2017

Re: Force remove power off zigbee node?!

Since you device is powered off, it's no way to receive a leave request from its parent. You have to implement a button press to do factory reset otherwise the device still can send data in original network.