Reply
Posts: 2
Registered: ‎10-10-2017

Efr32bg1 pin connection

In the datasheet of the Efr32bg1 there is a typical connection diagram in section 5. However in this diagram the value of capacitance and inductance are not given. What are these values ? Also is this application circuit for using Efr32bg1 stand alone without the starter kit ? Can we use Efr32bg1 without starter kit ?

Posts: 93
Registered: ‎02-25-2014

Re: Efr32bg1 pin connection

Please see the HW design considerations in the following application note:

https://www.silabs.com/documents/public/application-notes/an0002.1-efr32-efm32-series-1-hardware-des...