Reply
Highlighted
Posts: 4
Registered: ‎08-11-2017

Choosing of development board/evaluation kit for BlueMesh and Zigbee

Hi all,

I'm thinking to buy SLWSTK6020B for BlueMesh and SLWSTK6000B for Zigbee, but unfortunatelly the total price is too high. Are there another ways how to test BlueMesh BGM111 and Zigbee MGM12P32 with 1 development board or evaluation kit? At general I want to create simple coordinator - endpoint data transfer. 

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 161
Registered: ‎02-13-2017

Re: Choosing of development board/evaluation kit for BlueMesh and Zigbee

SLWSTK6000B and SLWSTK6020B are the most cost effective EVB available. BGM111 and MGM12P32 are just modules and you still need BRD4001a if you want to do development.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen