Reply
Posts: 12
Registered: ‎06-04-2015

Can ZigBee not send broadcasts continuously?

Em3585 use the broadcast address 0xFFFF continuous send data, start several times can be successfully sent, after all did not send out, after a few seconds and then can be sent back, how to solve the problem can not be continuous broadcast?

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 181
Registered: ‎02-13-2017

Re: Can ZigBee not send broadcasts continuously?

It's not recommended to send broadcasts continuously. If you have lots of Zigbee routers in the network, it might cause broadcast storm and show the result as you observed.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen