Reply
Highlighted
Posts: 48
Registered: ‎11-07-2015
Accepted Solution

Are ARTIK 030 and MGM111 the same thing?

As I understand ARTIK 030 is a just rebrended MGM111. Am I right?

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero</font></font> </a> YK
Posts: 183
Registered: ‎02-13-2017

Re: Are ARTIK 030 and MGM111 the same thing?

According to data sheet, you are correct.

If my reply answers your question, please click on "Kudo"s or "Accept as Solution"s to benefit others who have the same issue.

YK Chen
Posts: 48
Registered: ‎11-07-2015

Re: Are ARTIK 030 and MGM111 the same thing?

ARTIK 030 and MGM111 the same thing based on EFR32MG1P132F256GM48

 

Also you can check my post in blog (on Russian)

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru