Missing files preventing NCP project Generation in ZNET 5.8.x

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> ADKates on ‎12-30-2016 01:11 PM

Question

I’m trying to base my ZigBee NCP project on one of the WSTK modules, using my own board design with the same pinout as an existing EFR32 module. When I pick the module board header as a “Custom header,” my project won’t compile because it can’t find several files like bspconfig.h. I’m not using Hardware Configurator. What should I do?

Answer

Add the following files to the Additional .c and .h files, include paths, libraries in the Other tab by clicking on Add directory... (not Add file...):

 

C:\SiliconLabs\SiliconLabsEmberZNet\5.8.12.0-ALPHA_2\hardware\kit\common\bsp

C:\SiliconLabs\SiliconLabsEmberZNet\5.8.12.0-ALPHA_2\hardware\kit\common\drivers

C:\SiliconLabs\SiliconLabsEmberZNet\5.8.12.0-ALPHA_2\hardware\kit\EFR32MG1_BRD4155A\config (use your part/board file)