Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> DW8
Posts: 14
Registered: ‎04-15-2016

where can I found "Types.h" in CP2110/4 Software package for Windows Version 6.7.4

When compiling CP2110/4 Software package for Windows Version 6.7.4 in Visual C++ 6.0, I got the following error: "Cannot find Types.h", I checked SLABHIDtoUART.h and find these lines:
 
"

...

#include "Types.h"

...

"
But where can I get the file "Types.h".

Posts: 2,218
Registered: ‎10-14-2014

Re: where can I found "Types.h" in CP2110/4 Software package for Windows Version 6.7.4

@DW8

 

After install the CP2110_4_Windows.exe package, I see the SLABHIDtoUART.h in folder CP2110_4_SDK\Library\Windows don't have the line to include types.h.

But the file for Linux and MAC include this line.

 

My views are my own and do not necessarily represent the views of Silicon Labs

WeiguoLu
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> DW8
Posts: 14
Registered: ‎04-15-2016

Re: where can I found "Types.h" in CP2110/4 Software package for Windows Version 6.7.4

@delu

 

I am using "CP2110/4 Software Development Kit Version 6.7.4 - Feb 1, 2017". The setup file is named "CP2110_4_Windows.exe" 1.png

Posts: 2,218
Registered: ‎10-14-2014

Re: where can I found "Types.h" in CP2110/4 Software package for Windows Version 6.7.4

@DW8

Yes, I see it now with the latest package installed.

It was strange. Suggest you create a ticket in our Salesforce system to check why it was lost in the package.

http://www.silabs.com/support/Pages/default.aspx

 

My views are my own and do not necessarily represent the views of Silicon Labs

WeiguoLu