Reply
Highlighted
Posts: 3
Registered: ‎05-15-2013

Using CP2101 with Mac OS X

My company has a product using the CP2101, and I’m working on porting our desktop library from Windows to Mac OS X. I understand how to treat a device file as a COM port under *nix, but I’m not sure which device file is set up for me by the Silicon Labs driver. Is there any documentation on this driver? Or at least some example code?
Posts: 294
Registered: ‎10-01-2003

Re: Using CP2101 with Mac OS X

This link should give you information on how to handle a serial device under OSX. Unfortunately it's very different from Windows, but the ideas are the same.

http://www.cmrr.umn.edu/~strupp/serial.html

After you install the OSX VCP driver it will show up as /dev/tty.SLAB_USBtoUART
Posts: 3
Registered: ‎05-15-2013

Re: Using CP2101 with Mac OS X

OK, thanks!