Reply
Newbie
Posts: 1
Registered: ‎06-16-2013

[SOLVED] cp2102 LOGO!Soft Comfort Debian Wheezy

Hi

New to forum so saying hi to all willing to help with my problem.

First things first:

Linux Debian 7 Wheezy x32 pretty much fresh install (about a week now)
Silicon Labs CP2102 USB to UART Bridge Controller

and trying to communicate with LOGO Soft Comfort (v6.1.12, v7.1.5 (newest)) to transfer data from my laptop to plc siemens LOGO.

So what i do is i connect cp2102 to usb port and


emvoo@debian:~$ dmesg
[32481.812091] usb 2-2: reset low-speed USB device number 2 using uhci_hcd
[33561.909578] usb 1-1: USB disconnect, device number 5
[33571.424096] usb 2-1: new full-speed USB device number 3 using uhci_hcd
[33571.583268] usb 2-1: New USB device found, idVendor=10c4, idProduct=ea60
[33571.583277] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[33571.583283] usb 2-1: Product: CP2102 USB to UART Bridge Controller
[33571.583288] usb 2-1: Manufacturer: Silicon Labs
[33571.583292] usb 2-1: SerialNumber: 0001
[33572.089982] usbcore: registered new interface driver usbserial
[33572.090004] USB Serial support registered for generic
[33572.090047] usbcore: registered new interface driver usbserial_generic
[33572.090050] usbserial: USB Serial Driver core
[33572.094727] USB Serial support registered for cp210x
[33572.094769] cp210x 2-1:1.0: cp210x converter detected
[33572.204096] usb 2-1: reset full-speed USB device number 3 using uhci_hcd
[33572.349867] usb 2-1: cp210x converter now attached to ttyUSB0
[33572.349912] usbcore: registered new interface driver cp210x
[33572.349917] cp210x: v0.09:robotfrustrated:ilicon Labs CP210x RS232 serial adaptor driver
[33731.144206] usb 2-1: USB disconnect, device number 3
[33731.144722] cp210x ttyUSB0: cp210x converter now disconnected from ttyUSB0
[33731.144755] cp210x 2-1:1.0: device disconnected
[33762.880100] usb 2-1: new full-speed USB device number 4 using uhci_hcd
[33763.040468] usb 2-1: New USB device found, idVendor=10c4, idProduct=ea60
[33763.040477] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[33763.040483] usb 2-1: Product: CP2102 USB to UART Bridge Controller
[33763.040488] usb 2-1: Manufacturer: Silicon Labs
[33763.040492] usb 2-1: SerialNumber: 0001
[33763.045534] cp210x 2-1:1.0: cp210x converter detected
[33763.156161] usb 2-1: reset full-speed USB device number 4 using uhci_hcd
[33763.301899] usb 2-1: cp210x converter now attached to ttyUSB0
[33778.264200] usb 2-1: USB disconnect, device number 4
[33778.264706] cp210x ttyUSB0: cp210x converter now disconnected from ttyUSB0
[33778.264738] cp210x 2-1:1.0: device disconnected
[33793.384136] usb 2-1: new full-speed USB device number 5 using uhci_hcd
[33793.541477] usb 2-1: New USB device found, idVendor=10c4, idProduct=ea60
[33793.541485] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[33793.541491] usb 2-1: Product: CP2102 USB to UART Bridge Controller
[33793.541496] usb 2-1: Manufacturer: Silicon Labs
[33793.541501] usb 2-1: SerialNumber: 0001
[33793.546544] cp210x 2-1:1.0: cp210x converter detected
[33793.656153] usb 2-1: reset full-speed USB device number 5 using uhci_hcd
[33793.797067] usb 2-1: cp210x converter now attached to ttyUSB0


so it seems debian is recognising the cable but when i


emvoo@debian:~$ sh ~/logo_soft_comfort/LOGOComfort


it opens LOGO Soft Comfort then i go to Options -> Interface nothing is there so i click on automatic detection and get an error

'Interface selection error
Please check:
-Mode of the LOGO!:robottongue:C <-->LOGO!
-The LOGO!PC cable connects the LOGO! and the PC'

But i know for sure that both are fulfilled. I also know that cable is working properly (as it worked under windows before i installed debian and worked once or twice under ubuntu (just before debian - main reason i switched to debian was that cable stopped working in ubuntu).

What could be the reason that LOGO Soft doesnt see (i mean it does when linux allows it (yes i blame linux as i managed to get it to work on win7 x64 even today) or cant communicate with cable. Even windows run under VM doesnt recognize cable at all (like nothing was connected) so i assume that linux somehow is blocking ttyUSB - but i dont know how to check/fix it.

Is there anyone who could advise/guide me on that matter please?

Thanks in advance

---------------------

Works now! All it was i had to start logo soft comfort as root as normal user didnt have access to ttyUSB0 and that makes me laugh really as im working on it for over a week now hahaha
Community Moderator
Posts: 16
Registered: ‎04-08-2013

Re: [SOLVED] cp2102 LOGO!Soft Comfort Debian Wheezy

Glad to see you found a solution.