Reply
Posts: 5
Registered: ‎03-24-2017

Problem with CP210x drivers for Windows 10

I have a Zedboard Zynq7000 and have been unable to get console output successfully on Windows 10 machine.

 

So Installed cp210x drivers but still unable to see any UART output in MobaXterm thru serial COM1 port.

I tried with both serial enum driver and the default option. Rebooting between each attempt.

 

I do not see any new COM device listed when pwoering up the Zedboard. I also ried to in manually and try to force Windows to load the install slabvcp driver for one of the HID USB input devices listed but windows does not allow.

 

I am attaching the Device manager screenshot.

 

Posts: 429
Registered: ‎02-21-2014

Re: Problem with CP210x drivers for Windows 10

I would recommend taking a walk through this article: http://community.silabs.com/t5/Interface-Knowledge-Base/Troubleshooting-a-Product-Using-a-CP210x-USB...

 

It may have some information that can solve your problem.

Posts: 5
Registered: ‎03-24-2017

Re: Problem with CP210x drivers for Windows 10

Thank you, it was very helpful.

The problem was on my end, inadvertently I started connecting to the (JTAG) Prog port in the Zedboard instead of the UART USB port.

They are very close together jeje.