Reply
Posts: 2
Registered: ‎09-06-2017
Accepted Solution

Mac OSX Updating Driver

Hello,

 

I'm on version 4.10.17  having some intermittent issues.

 

I see I am a few versions back and will try to go to the latest and see if that helps.

 

Question: Do i have to uninstall the current version or an I just install the new version?

 

If i need to uninstall, any quick suggestions on how to do that. I read about running the uninstaller script, but not sure I know where that is.

 

Thanks...

Highlighted
Posts: 371
Registered: ‎09-04-2013

Re: Mac OSX Updating Driver

To uninstall the VCP driver on Mac OS, you may refer to the KB article below:

http://community.silabs.com/t5/Interface-Knowledge-Base/Uninstall-VCP-Driver-on-Mac-OS/ta-p/111945

 

The latest VCP driver for Mac is 5.0.1, which can be downloaded from link below:

https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers