Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> Del
Posts: 1
Registered: ‎02-27-2015

Looking for a cp210xVCP driver for CE7 (Windows Embedded Compact 7).

I check the download site and found the drivers for CE5 and CE6, but none for CE7.  Are there any plans to release a driver for the CE7 platform?  If not what options are available?

 

Thanks

Del

Posts: 530
Registered: ‎10-12-2004

Re: Looking for a cp210xVCP driver for CE7 (Windows Embedded Compact 7).

Hi Del,

 

We don't currently have one, and we don't currently have it on the roadmap.  It would be possible to create one, though, based on the AN571 CP210x interface specification:

 

https://www.silabs.com/Support%20Documents/TechnicalDocs/AN571.pdf

 

~Tabi

Tabitha Parker
MCU Applications and Support Manager
Silicon Laboratories