Reply
Highlighted
Posts: 2
Registered: ‎04-12-2016

Cant find SLABCP2112.cs

[ Edited ]

Hi,

 

I've just been asked to knock up an application using the CP2112 EK board, and have downloaded the Windows package for it.

 

We predominantly code in C#.net, and in AN496 in mentions a SLABCP2112.cs which I presume is the import declarations for the DLLs, but this file is not present in the latest Windows Package.

 

I could manually create my own from the C++ header files, but with so many imports and all the types, I'd appreciate it if someone had a copy of the .cs file so I can save some time.

 

Regards,,

 

Phil

Posts: 2
Registered: ‎04-12-2016

Re: Cant find SLABCP2112.cs

Someone had a previous version of the windows package that had this file, and sure enough has all the imports defined! Which all seem to be working.

Posts: 381
Registered: ‎09-04-2013

Re: Cant find SLABCP2112.cs

Please download the CP2112 software package for Windows from link below:

 

http://www.silabs.com/products/interface/Pages/interface-software.aspx#cp2112

 

Then install it, and you should see the SLABCP2112.cs under your installation directory, in CP2112\Library folder.

Posts: 3
Registered: ‎03-02-2016

Re: Cant find SLABCP2112.cs

I'm looking for the same thing (the C# import libraries for the CP2112 SDK).  I followed the link, installed the SDK, and I can't find any *.cs file anywhere in the installation folder.  

 

The installer reports that it is file version 14.0.0.0, and the installer name is CP2112_Windows.exe.

 

What am I missing?

 

Cheers,

 

Brain LeLacheru

 

 

Posts: 381
Registered: ‎09-04-2013

Re: Cant find SLABCP2112.cs

[ Edited ]

Sorry. Looks like the latest CP2112 SDK (version 6.7.2) for windows does not include SLABCP2112.cs and SLABCP2112.vb.

 

I enclosed the Library from an old CP2112 SDK v1.0 here for your reference, please change the attachment as a zip file type and then extract it.

Posts: 1
Registered: ‎06-08-2017

Re: Cant find SLABCP2112.cs

Hello, 

We want to use Windows 10 IoT Core for all our future products.

https://developer.microsoft.com/en-us/windows/iot/docs/buildingappsforiotcore

Language of choice is C#.

We decided to use SILAB CP2112 because of price and C# support.

Please let me know when you will reintroduce support for C# managed code?

Note: in latest version v6.7.4 SLABCP2112.cs is still missing

Posts: 2,384
Registered: ‎10-14-2014

Re: Cant find SLABCP2112.cs

I suggest you create a ticket in our salesforce to check if this is still available.

http://www.silabs.com/support/Pages/default.aspx

 

My views are my own and do not necessarily represent the views of Silicon Labs

WeiguoLu