Reply
Highlighted
Posts: 30
Registered: ‎09-23-2016

CP2114 B02 device as a Micro controller?

Dear Friends,

 

Can I use CP2114 B02 device as a Micro controller?.

In particular I want to modify my codec config based on GPIO input  on CP2114 B02,from the user. Also I donot want to do the same via any application running on PC. I want CP2114 to excecute this flow.

 

I could not find this in any documentation, Please suggest if there is a way.

 

Regards,

Vijayendra 

Posts: 1,733
Registered: ‎10-14-2014

Re: CP2114 B02 device as a Micro controller?

@vj_1987

I don't think this is possible on CP2114.

Maybe below KB helps, not sure if this option mentioned in the KB is ok for you.

http://community.silabs.com/t5/Interface-Knowledge-Base/CP2114-Switching-Configurations-on-the-fly/t...

WeiguoLu