Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> Jos
Posts: 1
Registered: ‎06-05-2013

CP2112 HidSmbus_WriteRequest() function

Hi,

How send more than 61 data bytes in one SMBus transaction?

HidSmbus_WriteRequest() function can send 61 bytes,
I need to transfer 75 bytes, if I'm trying to pass for two times,
the device receives the data as different commands.


Thanks.
Highlighted
Posts: 46
Registered: ‎04-30-2004

Re: CP2112 HidSmbus_WriteRequest() function

Hi Konstantin - the CP2112 devices are limited to 61 bytes in a single transfer.