USBXpress SDK Installer

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Stephen on ‎10-02-2017 02:07 PM

Question

Where can I find the USBXpress SDK installer? For example, the installer that contains SiUSBXp.dll, SiUSBXp.h, etc 

Answer

The USBXpress webpage and installer is now refers to USBXpress as Direct Access Drivers.

 

The installer can be found here:

https://www.silabs.com/products/development-tools/software/direct-access-drivers

 

After installation, the USBXpress SDK files will be located at this default location:

C:\SiliconLabs\MCU\USBXpress_SDK

 

The host side API has not changed, i.e. functions names are remain SI_Write() and SI_Read().

 

For 8-bit MCUs, the device side API has not changed.