Manually Install WinUsb Driver on Windows 7

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Jiehui on ‎02-06-2017 12:19 AM

Win7 ships with the correct 'winusb.sys' file, but is missing an updated '.inf' file that associates the driver with "usb\ms_comp_winusb" devices. Normally if the USB device supports Microsoft OS descriptors, then it will allow Windows to automatically install the WinUSB driver. This mechanism is supported "in-box" for Win8 and newer. For Win7 the mechanism is supported through Windows update. Depending on the update policy for the Win7 machine, the appropriate driver may or may not be already available on the machine. If it is not already on the machine, user can use the following manual procedure to install the driver if necessary.

 

  1. Search for "windows phone winusb" at [Microsoft®Update Catalog|https://www.catalog.update.microsoft.com/Home.aspx].
  2. Download "Windows Phone - Other hardware - WinUsb Device".
  3. Extract the contents of the downloaded '.cab' file to a temporary folder.
  4. In device manager select "Update driver software ..." --> "Browse my computer for driver software".

5. Navigate to the temporary folder with the downloaded driver and complete the installation.

 

This procedure only needs to be done once.