Default configurations for CP21xx command-line programming tools

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> BrianL on ‎06-12-2017 04:59 PM

In AN721SW.zip there exist standalone manufacturing tools that can be used to program CP21xx devices. This is described in section 4.1 of the AN721 application note. Attached to this article is a zip file that contains the default configurations for all programmable CP21xx devices:

 

  • CP2101
  • CP2102
  • CP2102n
  • CP2103
  • CP2104
  • CP2105
  • CP2108
  • CP2109
  • CP2110
  • CP2112
  • CP2130